3/2/2018 5:55 PM | |
Joined: 2/19/2007 Last visit: 9/11/2024 Posts: 10 Rating:
|
Hi TIBI68 I am using your MBMA340 library (CP340-RS485) with excellent results to communicate with 70 Danfoss VLT FC051. Congratulations for the excellent work. It is very easy and powerful. I am facing a problem in reading a holding register that contains the motor current. The register can be found at 16140. I understood that with your work you can read up to address 9999, as per the original modbus specifications. Correct? Can you help me? Regards
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/19/2018 9:06:03 AMNew subject after splitting |
|
This contribution was helpful to
1 thankful Users |
Follow us on