12/21/2023 11:36 AM | |
Joined: 5/6/2022 Last visit: 6/25/2024 Posts: 424 Rating:
|
Hi Homerjey, In the situation you find yourself in, I think you have no choice but to continue trying the method that you discuss in the second part with the USB. I would try other USBs to see if it is a problem that it is not being recognized. Because apart from this method there is only Prosave and Proneta, but both from what I see do not work due to the protection of the screen. There are no more reset options... Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on