2/25/2019 3:55 PM | |
Joined: 8/1/2017 Last visit: 5/14/2024 Posts: 10 Rating: (0) |
hello everyone! I have a problem with finding a way to upgrade my offline TIA project hardware configuration with the correct firmware for F-DI and F-DQ IO modules. Specifically: 6ES7 526-1BH00-0AB0, and 6ES7 526-2BF00-0AB0. For both of them I found the firmware update to version 1.0.2 here: https://support.industry.siemens.com/cs/de/en/view/109742146 https://support.industry.siemens.com/cs/de/en/view/109746436 When I go online I can see that theese modules have firmware version 1.0.2 but in my offline TIA project the firmware version remains 1.0 and I can't find a way to change to 1.0.2. I am using TIA portal V15.1 with the latest updates to hardware catalog. I would like to know how to change firmware version of these two IO modules in my offline project to 1.0.2. Also, the reason why upgrade to firmware 1.0.2 was necessary is that the old firmware caused communication error diagnostic message which would result in passivation of the IO module. This is a big issue, and I am not sure is it resolved by updating firmware of the IO module or I also need to change firmware version in the offline project and download the hardware configuration to PLC again to be sure the issue with communication error is resolved. Any clarification about this concern or suggestions on how to update firmware in the offline TIA project will be much appreciated. |
2/25/2019 4:02 PM | |
Joined: 5/12/2006 Last visit: 7/11/2024 Posts: 22308 Rating: (2998) |
hello, you need no update in the offline project. the version 1.0 is valid for V1.0.x. Regards Christoph |
2/25/2019 4:41 PM | |
Joined: 5/12/2006 Last visit: 7/11/2024 Posts: 22308 Rating: (2998) |
hello, no this is not possible.
Christoph |
Follow us on