Industry Online Support
Technical Forum
6/15/2010 10:08 AM | |
Joined: 3/24/2009 Last visit: 6/20/2023 Posts: 535 Rating: (112) |
Dear PRADEEP PRABHU, ad 1) for the monitoring-time have a look at this link (tab min. F-Monitoring times). You have to define the value in the HW-Configuration. It must be higher as the cycletime of the calling OB. ad 2) did you set the DIP-switch of the module to the correct adress? Best regards, yy1 |
Last edited by: yy1 at: 6/15/2010 10:25 AM |
|
6/29/2010 2:03 AM | |
Posts: 15 Rating: (2) |
Try increasing your F-Monitoring time, also make sure the network scan time is not too fast especially if you have a large and/or wireless network |
Follow us on