6/7/2018 11:09 AM | |
Posts: 1283 Rating:
|
Can you share your project file? I can help to check it with the LOGO? Jay |
6/7/2018 11:14 AM | |
Joined: 12/18/2014 Last visit: 8/6/2024 Posts: 33498 Rating:
|
Which version of the software LSC you are using? |
6/7/2018 1:16 PM | |
Posts: 1283 Rating:
|
I asked for the project file to understand the settings of the LOGO and everything. Not about the logic. Jay |
6/7/2018 1:44 PM | |
Joined: 12/18/2014 Last visit: 8/6/2024 Posts: 33498 Rating:
|
Hello GOG, your software version is V8.0.0. This version is not suitable for a LOGO! with firmware version V1.81.02. A LOGO! with firmware version V1.81.02 is a LOGO! 8.1 FS05 and a LOGO! 8.FS04 must be set in the hardware selection. With LSC V8.0 you can only program LOGO! S with firmware V1.08.01 to V1.08.03 (FS01 - FS03). You can download the upgrade to V8.2 here: Demo software , upgrades/updates, Drivers Please note, there are 2 versions for 32 Windows: 32bit and 64bit. After downloading you will receive a file called "Setup.exe". |
6/7/2018 1:48 PM | |
Posts: 1283 Rating:
|
hello ixo65, But he mentioned this as below, I'm using LOGO PLC6ED1 052-1FB00-0BA8 FW: V1.08.01, I've a problem with loading the program to the LOGO although the connection is established between the PC and the LOGO. which means he is facing issue with the lower version. he said higher version worked well. Correct me if i am wrong. Thanks, Jay |
6/7/2018 2:57 PM | |
Joined: 12/18/2014 Last visit: 8/6/2024 Posts: 33498 Rating:
|
I did some research in my old topics. At November 2016, I found the following. Bug durch LSC V8.1? It then comes to the error message "Error loading the panel". If you acknowledge the message, different things happen, depending on the program. I have the program open as V3 and determine the first error representation. Then changed the program several times, deleted blocks and inserted UDFs. That's the V6. In the simulation and in the real LOGO! 0BA8.Standard work the programs error-free, it just can not select the hardware." See attached videos. AttachmentFailed to load panel.zip (110 Downloads) |
Follow us on