2/24/2015 12:16 AM | |
Posts: 9 Rating: (0) |
Hello, I need help cause i've tried everything and don't know what to do. I have a logo!8 and a TDE, and they are connected by a ethernet cable, but my problem is that, TDE doesn't do nothing when logo is running. For example i tried a simple program with an entrance, a flag(TDE backlight RED) and a output, and everything works expect the backlight change. When i try to check LOGO! Settings on TDE, the same error appears on all of them : Error:Failed to submit Please help me ! Thank you AttachmentIMG_1494.MOV (213 Downloads) |
2/24/2015 12:00 PM | |
Posts: 9 Rating: (0) |
How can i do that? |
2/24/2015 3:29 PM | |
Joined: 12/18/2014 Last visit: 7/21/2024 Posts: 33382 Rating: (4143) |
Look at attachment. |
2/24/2015 7:23 PM | |
Posts: 9 Rating: (0) |
I've tried all that appear and still doesn't work |
2/24/2015 8:54 PM | |
Joined: 12/18/2014 Last visit: 7/21/2024 Posts: 33382 Rating: (4143) |
Has the TDE an IP address? |
2/24/2015 9:06 PM | |
Posts: 9 Rating: (0) |
this is what i've been trying AttachmentIMG_1498.MOV (264 Downloads) |
2/24/2015 9:29 PM | |
Posts: 9 Rating: (0) |
thanks anyway for the attention |
This contribution was helpful to1 thankful Users |
Follow us on