12/21/2006 8:20 PM | |
Joined: 12/18/2006 Last visit: 6/20/2024 Posts: 19 Rating: (2) |
Hi Dellok, Will “Report System Error” do the job? See:
http://support.automation.siemens.com/WW/view/en/22727528 Dolf |
12/22/2006 10:00 AM | |
Joined: 4/24/2006 Last visit: 7/10/2024 Posts: 8711 Rating: (1165) |
Hello dellok, I think your I/O card is passivated. And you should reïntegrate it Have you seen following faq: http://support.automation.siemens.com/WW/view/en/22304119 Here is link to manual: http://support.automation.siemens.com/WW/view/en/19026151 See chapter 7.2.2 Perhaps this will help. Merry Christmas Wizard |
12/23/2006 6:22 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (316)
|
Hi Dellok, You may depassivate the F-I/O from your panel with the function F_ACK_OP {FB187}which in the F-library thats coming with distributed safety. See also the handbook S7 Distributed Safety - Configuring and Programming on chapter 9.1.2.9 this failsafe block is described. [:o] For depassivating you need the signal from the previous block with the ACK_REI of the F-I/O which is coming from the datablock thats with the I/O placed. When the QBAD signal goes then the ACK_REI will come. You couldn't see on the F-I/O on the front if the I/O is passivated, only when QBAD is stil there the Red SF-LED will light up. Siemens is working on it to make it that way that the SF-LED blinks when it is ready for reintegration (now the LED is out). [;)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
12/23/2006 6:27 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (316)
|
[quote user="dellok"]In the event of a wire-break, I can find out which channel has the problem by using the hardware diagnostics. However, the on-site operator will not have access to the hardware diagnostics.He only has a TP270 touchpanel. How do I access the information that will tell the operator which channel has the problem? Hi Dellok, With SFC59 you can readout the record 1 and or 2 where such information can be read out. This information you can find in the handbook Automation System S7-300 Fail-Safe Signal Modules in chapter A Diagnostic Data of the Signal Modules. When you can not program this block, please let me know and I send a UDT and the source to it. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on