4/15/2024 2:13 AM | |
Joined: 4/14/2024 Last visit: 4/16/2024 Posts: 4 Rating: (0) |
Good afternoon team I have two Siemens S7 400 PLCs, the no.0 was as master and when it failed, I found the backup no.1. To the no.0 I flashing all the led, to make the connection with step7 and make the diagnostic buffer appears as unavailable. I tried to connect unsuccessfully attached the (image shown), when connecting to PLC 1 indicates that due to a voltage variation took control, I continued to insist on the connection to make the diagnosis of buffer and mark no Diagnostic information (attached image). Do you recommend: That I replace the CPU? or Reset the flash drive, if so you have the procedure to do so. I appreciate your cooperation. Greetings... AttachmentPLC SIEMENS S7 400 CPU 412-3H.pdf (504 Downloads) |
Last edited by: Jen_Moderator at: 04/15/2024 11:22:01Text formatting optimized. |
|
4/15/2024 3:49 AM | |
Joined: 4/14/2024 Last visit: 4/16/2024 Posts: 4 Rating: (0) |
If Booth have V 4.5.2 |
4/15/2024 4:30 AM | |
Joined: 2/28/2023 Last visit: 9/27/2024 Posts: 39 Rating: (1) |
Yes |
Cheers. |
|
Follow us on