4/11/2024 11:17 AM | |
Joined: 5/6/2022 Last visit: 5/21/2024 Posts: 420 Rating: (83) |
Hi Gianni.ESD, If the addresses are correct and the S7-1200 security allows access to all the variables, the first thing I would recommend would be to regenerate the project by deleting the IM folder and compiling again ("How do I delete the IM folder of my TIA Portal project?") and/or regenerate the tags in the project. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
4/11/2024 12:51 PM | |
Joined: 3/19/2024 Last visit: 4/11/2024 Posts: 2 Rating: (0) |
Thank you this was helpful, the problem is solved. |
This contribution was helpful to1 thankful Users |
Follow us on