8/11/2020 9:01 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Please check which option Z (technology board) is installed on your drive system. F117 is related with technology board & in your case probably would be with communication. Please refer Fault F117 on simovert vc this post for more information. HTH |
8/11/2020 9:53 AM | |
Joined: 4/11/2017 Last visit: 11/17/2023 Posts: 2 Rating: (0) |
The technology board of drive C is T400. |
8/11/2020 11:45 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, What is the application? Is it winder, tension reel or crane hoisting? Have you checked your profibus cable, profibus connector, card for tightness? What was the problem with drive A? Was any firm ware updated? Please refer below posts which will help you to understand T400 function with drive. T400T400 programmingHow to connect the computer to the T400 technology card?HTH
|
Follow us on