8/22/2018 12:08 AM | |
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating:
|
Hello cotch; We appreciate you efforts to write in English, but for our better understanding of your problems it would be preferable that you try using an electronic translator such as Google Translate. To help you better, we need to know what CPU you are using, what programming software is used in the project, and what Safety package (such as S7-Distributed Safety) has been implemented for the safety application. Passivation is specific to Safety I/O modules. It happens when a Safety I/O module detects a safety fault; it then removes itself from the safety program, until it is re-integrated by special functions in the PLC. This is called depassivation. The following Safety Engineering manual will give you mu informtion on safety programs, I/POs and faults: SIMATIC Industrial Software Safety Engineering in SIMATIC S7 https://support.industry.siemens.com/cs/ww/en/view/12490443 ● Passivation of F-I/O/Channels of an F-I/O. F-I/O / channel faults or communication errors lead to passivation of the corresponding FI/O or F-I/O channels and the F-CPU does not go into STOP. Once faults are eliminated, the F-I/O or channels of the F-I/O must be reintegrated (depassivation). Reintegration (switchover from fail-safe values to process data) occurs automatically or, alternatively, after mandatory acknowledgment by the user. Standard diagnostic and message functions can also be implemented in response to a detected fault. Have a look at the following discussion and see if it resembles your situation. Tell me, do you have access and experience with your PLC program? Hope this helps, Note: Many of the links and documents we point to in our answers are available in other languages, including French. Simply change the Language selector in the download page for a manual. For example: SIMATIC Logiciel industriel Technique de sécurité dans SIMATIC S7 https://support.industry.siemens.com/cs/ww/fr/view/12490443 D.C. |
Last edited by: dchartier at: 8/22/2018 12:09:43 AMLast edited by: dchartier at: 8/22/2018 1:24:29 AMLast edited by: dchartier at: 8/22/2018 1:28:07 AM |
|
Follow us on