7/20/2016 9:23 PM | |
Posts: 93 Rating:
|
Hi all, We have two S7-400 PLC that CPU 416-2DP . I have doubt in the FC and FB calling OB-1. My Project details, CPU-1(LINE) : The CPU-1 using lot of FC and FB, but only FC is Called in the OB-1. FB is not called in the OB-1. CPU-2(STACKER) : The CPU-2 using Lot of FC and FB, but only FB is Called in the OB-1. FC is not called in the OB-1.(only three FC is called in OB-1). I can create new FB and FC in the both CPU, that new FB and FC not going to online mode. Pop up message displayed as block not found. Now I created new FB and FC is called in the OB-1. Now it's going to online mode. My doubt is 1.How that uncalled FB and FC is going to online mode in my Project? 2. in case create new FB and FC must or necessary need to call in OB-1 ? For better understanding of my doubt here I attached the file. pls go through it and reply me. Advance Thanks & Regards, Suryamuni. AttachmentOB-1 CALL DOUBT.pptx (281 Downloads) |
7/20/2016 10:19 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello, In short: If STEP 7 says "block not found " is because it is not loaded into the CPU , if a FB or an FC is not called in OB1 is because it will be called from another FC or FB , the UC calls of FB means a recall without parameters , maybe it's best that you read this manual: Have a look like chapter 4.2 and 4.2.2 for Hierarchy block and so on: https://support.industry.siemens.com/cs/attachments/18652056/S7prv54_e.pdf |
Last edited by: Ste39 at: 7/20/2016 10:31:46 PM |
|
7/22/2016 1:09 AM | |
Posts: 93 Rating:
|
Hi ste39, I cross referenced the FB-30, it's called in FC-72 and FC-221. In my program OB-35 is used. But FB-30 is not called in OB-35 and OB-1. here i attached the file for better understanding. Thanks & Regards, Suryamuni. Attachmentcross reference.pptx (269 Downloads) |
7/22/2016 11:22 PM | |
Posts: 93 Rating:
|
Hi, pls see that FB-30 call structure. Regards, Suryamuni. |
Follow us on