8/6/2012 3:31 PM | |
Joined: 10/26/2011 Last visit: 7/22/2024 Posts: 762 Rating:
|
Hello Phil_UK To FbDrive: - deinstall the Drive ES library - look for the right GSD file - Implement the motor via GSD file, not via object manager. After that, it should work. To Drive ES: Which version of Drive ES do you have? The Drive ES for PCS 7 Version 8 is availabe since 10.07.2012. The Drive ES for PCS 7 V7.x is not running in PCS 7 V8. For PCS 7 V8 there are two Drive ES versions available. One version for updateing from PCS 7 V7.x -> V8 And one version for PCS 7 V8 new engineering. In this version, you get only the Drive ES driver blocks and for operating and monitoring, you have to use the APL standard blocks. Messages: If you use the the Drive ES block behind a APL block, than you should deactivate the messages form the Drive ES block. Regards |
SIMATIC PCS 7 - Overview |
|
8/7/2012 10:01 AM | |
Joined: 10/26/2011 Last visit: 7/22/2024 Posts: 762 Rating:
|
I am a little bit confusing. There are two possibilities to integrate drives in PCS 7 Version 8. 1. To use the universal standard APL block "FbDrive". With this block you can implement all drives, which are using the standard telegramm 20. With this block you have the baisc funktionality of the frequency converter, start, stop, rotation frequency, current,effective power, ...) This block is included in the APL, needs not additional process object (PO) and no Drive ES library. In the APL library you find an example template for this solution. 2. If you want to have the complete frequency converter functionality, than you have to buy the Drive ES. For PCS 7 Version 8, there is a completly new Drive ES library available. NEW The Drive ES PCS 7 APL blocksareonly driver blocks and have no faceplates inclusive. For monitoring and operating, you have to use the standard APL motor block "MotSpdCL", not the "FbDrive". The new Drive ES block needs no additional process objects (PO) and there are no double messages. Additional all the warning numbersand fault numbers from the frequency converter are displayed in the APL standard MotSpdCL block symbol, in the faceplate and inthe OS Runtime "One Alarm Line". The document "Configuration of SINAMICS and MICROMASTER Drives with Drive ES in PCS 7" http://support.automation.siemens.com/WW/view/en/58007228describes this solution. At the moment it is only available for PCS 7 V7.1, but it is in the updating process and will available for PCS 7 V8 as soon as possible. |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to
2 thankful Users |
10/22/2012 1:08 PM | |
Joined: 10/26/2011 Last visit: 7/22/2024 Posts: 762 Rating:
|
Hello, The FbDrive is a driver block, but it is differnet to the APL_GS and APL_G120. The FbDrive is for all frequency converters, the APL_GS / G120 only for Siemens Drives. The FbDrive has a liitle bit mor functionality, then a pure driver block. You have additional the error number of the frequency motor, a new add-on faceplate, which you can open via the MotSpdCL faceplate and you can connect all frequency drives. The APL_GS / G120 driver blocks, have more functionality then the FbDrive. You can connect these blocks with the statistic blocks (also in the DriveES library). And you can use all the features, which the Siemens drives have inside. |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to
2 thankful Users |
9/8/2016 1:31 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
New question published by AutoGen_295051 is split to a separate thread with the subject G120 and PCS7 8.1 SP1 using DRVPCS7 APL 8.1 block FB1721, problem with speed reference. Best regards |
Follow us on