10/18/2023 5:22 PM | |
Joined: 10/18/2023 Last visit: 10/18/2023 Posts: 6 Rating: (0) |
hello, I have a cecc-d plc by festo, i need work this whit a logo by siemens, festo as master and logo as slave, i made the configuration same a festo-siemens s1200, but doesn´t work. It´s possible ? thank you file:///C:/SOFTWARE/ModbusTCP_Codesys_Siemens.pdf ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/19/2023 08:10:03New subject after splitting |
|
10/18/2023 5:34 PM | |
Joined: 12/18/2014 Last visit: 6/30/2024 Posts: 33263 Rating: (4115)
|
The link don't work. |
10/18/2023 7:20 PM | |
Joined: 12/18/2014 Last visit: 6/30/2024 Posts: 33263 Rating: (4115)
|
I'm sorry, but I don't know nothing about codesys. |
10/18/2023 7:23 PM | |
Joined: 10/18/2023 Last visit: 10/18/2023 Posts: 6 Rating: (0) |
about logo ? it´s posible that work in this case or only work whit siemens plc´s ? |
10/18/2023 7:32 PM | |
Joined: 12/18/2014 Last visit: 6/30/2024 Posts: 33263 Rating: (4115)
|
The example is for Siemens PLC S7. The LOGO! can't use the blocks of the S7 and the communication of LOGO! is other. The LOGO! 8.1 or newer can only Modbus TCP/IP. Speaks the modbus controller also Modbus TCP/IP? |
10/18/2023 7:36 PM | |
Joined: 10/18/2023 Last visit: 10/18/2023 Posts: 6 Rating: (0) |
I do have the logo 8.1, and I need it to work as an extension of inputs and outputs, through modbus communication. And that its inputs and outputs can be controlled by the CECC-D plc. |
10/18/2023 7:44 PM | |
Joined: 12/18/2014 Last visit: 6/30/2024 Posts: 33263 Rating: (4115)
|
I think this is not possible with the LOGO!. The LOGO! can't make the communication as the S7. The LOGO! can only read or write modbus addresses directly. Can you tell me what the LOGO! have to read (IR,HR, Coils etc)? I don't know. |
10/18/2023 7:46 PM | |
Joined: 10/18/2023 Last visit: 10/18/2023 Posts: 6 Rating: (0) |
Logo is conect to digital sensor 24 vc, push buttons and the output are conect to selenoid valve, all signals are digital. |
10/18/2023 7:49 PM | |
Joined: 12/18/2014 Last visit: 6/30/2024 Posts: 33263 Rating: (4115)
|
I'm sorry, I can't help you in this case. It seems like we're talking past each other. |
Follow us on