5/15/2016 9:43 AM | |
Posts: 8946 Rating:
|
Hello fellow colleagues, quite fresh we get Siemens announcement the new Field PG M5. https://support.industry.siemens.com/cs/ww/en/view/109483458
Does anyone perhaps have seen the new PG M5 in action? Evt. at a trade show? If the fan is still in chain saw volume? How then does the S5 option work, dual boot is probably no longer available? What is the display? 1920 x 1080 legible?
|
This contribution was helpful to
2 thankful Users |
5/15/2016 10:58 AM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating:
|
Hello Jürgen, Thanks for the fresh tip. I can't answer all of your questions but you may have a look on the video in this link and compare the fan size to the one of M4. Note: if you check the brochure (in the same link) you will see it supports full HD 1920X1080. Best regards, H-H |
This contribution was helpful to
2 thankful Users |
5/15/2016 11:50 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello Juergen, This below is in Italian language but with Google... however, it says that the screen will be Full HD 15.6 " and there will be two versions, the Advanced will support S5 , if I have other information will be a pleasure give to you . http://automazione-plus.it/notebook-industriali-robusti-simatic-field-pg-m5_83470/ |
This contribution was helpful to
1 thankful Users |
Follow us on