Industry Online Support
Technical Forum
11/6/2014 3:12 PM | |
Joined: 7/2/2008 Last visit: 5/16/2024 Posts: 928 Rating: (306) |
Hellokinjalpatel1899, The answer depends on some parameters like the available effective surface area, maximum available internal and external temperature. The easiest way (for me) would be using the Rittal Therm software. Even if you don't have Rittal panels, you still can use Rittal panels with similar dimensions just for calculation. I also recommend to read the"Project Planning Manual - Enclosure Heat Dissipation" from Rittal. Best regards, H-H
|
Follow us on