Industry Online Support
Technical Forum
9/3/2008 3:39 PM | |
Posts: 3 Rating:
|
Dear All, My plant have a hydraulic system as following: -Input: Displacement transducer: Micropulse of balluff, BTL5-P2-M0150-B-S32, Vus=2838,99m/s -One axis controller: EMC -Output: propotional valve with +-20mA input This controller get demand and setpoint to choose 1 in 100 profiles that was programed in EMC100 memory from MCS(S7-CPU315-2 DP). A one axis controller(EMC100 Parker) control grate of clinker cooler. We could not buy it. We want to find a simotion controller. to replace above EMC100. Please recommend us how to choose the best simotion controller. Thanks. HT Profile see attach AttachmentEMC080204_V1.10.ZIP (466 Downloads) |
9/3/2008 5:11 PM | |
Posts: 116 Rating:
|
Hi, see https://www.siemens.com/simotion for an overview. See catalog for detailed information: https://mall.automation.siemens.com/DE/guest/ -->Products -> Automation Systems -> SIMOTION Motion Control System -> ... FAQ about a hydraulic application with D410: http://support.automation.siemens.com/WW/view/en/28017319 Ciao Jerry |
Follow us on