4/29/2020 8:29 PM | |
Posts: 2 Rating: (0) |
I am currently working on a project in tia portal V14, I registered the CPU 1511 model 6ES7 511-1AK01-0AB0 with firmware version 2.1, part number with which I had always worked correctly. The problem is that the new generation CPU 1511 had a change in the part number, it is now 6ES7 511-1AK02-0AB0 and it comes with firmware 2.8, this previous part number does not appear in the device catalog in the portal V14. My question is the following: Is there an option to work on this new generation CPU with the aunt portal v14? or to which version of aunt do I have to migrate? I understand that in the V15 version of the aunt portal if the part number of the plc appears but it goes up to firmware 2.5 Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/30/2020 06:19:14New subject after splitting |
|
Follow us on