6/7/2011 11:25 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating:
|
Hi lordgalen, In the Following Link it is mention. Downgrading to an older firmware version: In the case of a CPU417-4H (order no. 6ES7 417-4HL01-0AB0) with test date R, S or T, a downgrade can be performed to not lower than version V3.0.0. You can identify the test date by the yellow test label on the rear side of the module. The test date is in the second line under SIEMENS/TESTED, behind VP. If a downgrade is required for your installation and the above restriction is applicable, please contact your local Siemens office. I know you are using the CPU 414H ..... can you tell me why you want to Downgrad the Firmware ? |
Ammy |
|
6/8/2011 3:02 PM | |
Posts: 947 Rating:
|
HI I think, you make downgrade,if load all need file to flash (make update by flash) |
6/9/2011 7:07 AM | |
Joined: 4/22/2010 Last visit: 6/5/2024 Posts: 82 Rating:
|
Hi Aret, Thansk you so much for your answers..Anway what is MLFB? Thanks and best regards, lordgalen
|
6/9/2011 7:22 PM | |
Posts: 947 Rating:
|
Hi lordgalen I would recommend are all set (install) firmware 4.0.12 on both CPU |
Follow us on