Industry Online Support
Technical Forum
7/26/2013 10:14 AM | |
Posts: 28 Rating: (0) |
is it needed siemens sd card for updating new firmware to plc? Could be done updating new firmware to plc without siemens sd card?
|
7/26/2013 10:57 AM | |
Posts: 378 Rating: (47) |
Hello, usually you need one. I know only one possibility where you don´t need one. And this is only possible when you have TIA V12 and S7-1200 PLC with Firmwareversion V3.0 or higher. http://support.automation.siemens.com/WW/view/en/67190848 Best regards Bilao |
7/26/2013 11:00 AM | |
Posts: 461 Rating: (29) |
Yes u must have siemens memory card for firmware update( through mc card) , check the attached pdf as reference for firmware update ... upgrade process --\ https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=38710101&nodeid0=41886031&load=content&subtype=133100&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW Regards, Nelliyan.G Attachments71200_firmware_update.pdf (1444 Downloads) |
Last edited by: Nelliyan randy at: 7/26/2013 11:03 AM |
|
Follow us on