2/1/2022 5:05 PM | |
Joined: 4/28/2015 Last visit: 11/29/2023 Posts: 3289 Rating:
|
Hi folks, a new firmware for PG1 devices of IOT2050 Basic (FS:01) and IOT2050 Advanced (FS:01, FS:02, FS:03) has been released.
It is required to perform the firmware update with Example Image V1.1.1. Instructions and required files are attached to this post and can be found here as well. PG2 devices of IOT2050 Basic (from FS:02) and IOT2050 Advanced (from FS:04) are running on new firmware from factory. Overview about firmware and Example Image combinations: IOT2050 Basic
IOT2050 Advanced
EDIT: How to document has been updated to V1.3 as well as the firmware version. Changelog: Added requirement to clear eMMc before updating the firmware, when Example Image V1.0.2 or Industrial OS V2.x is installed on the eMMc of IOT2050 Advanced EDIT: How to document has been updated to V1.3.1. Best regards! AttachmentIOT2050_Firmware_Update_Files_V1.3.1.zip (14 Downloads) |
Last edited by: bergmanu at: 03/09/2022 11:22:27updated PDF to V1.1 Last edited by: bergmanu at: 03/15/2022 07:28:42Last edited by: bergmanu at: 04/20/2022 07:40:31Last edited by: bergmanu at: 01/09/2023 06:53:25added Industrial OS Last edited by: bergmanu at: 05/10/2023 01:56:20Last edited by: bergmanu at: 11/20/2023 15:00:35Last edited by: bergmanu at: 11/20/2023 15:12:46 |
|
This contribution was helpful to
4 thankful Users |
Follow us on