12/21/2018 6:44 PM | |
Joined: 12/18/2014 Last visit: 4/18/2025 Posts: 35132 Rating:
|
Firmware update V2.1.5 for LOGO! CMR2020 (6GK7142-7BX00-0AX0) and LOGO! CMR2040 (6GK7142-7EX00-0AX0) The new firmware V2.1.5 for the LOGO! CMR2020 and LOGO! CMR2040 modules has been released and is now available for download free of charge. Firmware version V2.1.5 is the successor to version V2.1.4 and contains important product improvements. Upgrading with a free firmware update is recommended. The LOGO! CMR2020 and LOGO! CMR2040 with firmware V1.x or V2.x that are already in use can be updated via the Web Based Management (WBM). The LOGO! CMR2020 (6GK7142-7BX00-0AX0) and LOGO! CMR2040 (6GK7142-7EX00-0AX0) modules are scheduled to be delivered with the new firmware V2.1.5 as soon as possible. |
This contribution was helpful to
3 thankful Users |
Follow us on