10/8/2019 6:05 AM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32895 Rating: (4067)
|
Firmware update V2.1.7 for LOGO! CMR2020 (6GK7142-7BX00-0AX0) and LOGO! CMR2040 (6GK7142-7EX00-0AX0) 2.Produktverbesserungen LOGO! CMR2040: Time synchronization via GPS: Affects all systems connected with a LOGO! CMR2040 update the assembly time via GPS. Due to the overflow of a counter in the GPS receiver (GPS rollover), there will be incorrect GPS time synchronization from 2 November 2019 at 23:59:42 UTC with older firmware versions. Upgrading to FW V2.1.7 is strongly recommended for this application. The CMR2020 is not affected. Communication via VPN: The data throughput via the VPN connection of the LOGO! CMR2040 has been increased. SMS transmission: The sporadic behavior that after upgrading the FW from V1.x to V2.x no SMS could be sent has been fixed.
SMS user group: The behavior that SMS messages were incorrectly sent to user groups 1 and 2 instead of user groups 9 and 10 has been fixed. Name resolution (DNS): The name resolution for time synchronization via NTP, DynDNS and e-mail has been improved. Please note: At the moment, the language selection on this website does not work. Therefore, the contribution is only available in German. |
This contribution was helpful to2 thankful Users |
Follow us on