2/8/2022 11:58 AM | ||||||||
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi GoAu, have a look to the TIA help for the MB_Client instruction:
check this remedies. hope this helps, regards, |
|||||||
FCK WAR! |
||||||||
2/8/2022 5:03 PM | ||||||||
Joined: 2/23/2017 Last visit: 10/26/2023 Posts: 46 Rating:
|
hello mop_S04 , does it mean that I have my addressing incorrect or block is incorrectly assigned . I've attached a snap on of a FLIR AX8 manual and register i'd like to read if you could please take a look if i making mistake in addressing of a MB_Client or DB_values attached to the block . first picture is from FLIR manual and it represents a register from 401017-401037 length 20 Words second picture is my OB1 with a MB client and DB values.
hi GoAu, have a look to the TIA help for the MB_Client instruction:
check this remedies. hope this helps, regards, |
|||||||
2/8/2022 5:04 PM | |
Joined: 2/23/2017 Last visit: 10/26/2023 Posts: 46 Rating:
|
and a second pict . Regards GoAu |
2/9/2022 4:25 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
The block is complaining about the MB_DATA_PTR . so DB33 would also be interessting |
FCK WAR! |
|
2/9/2022 8:59 PM | |
Joined: 2/23/2017 Last visit: 10/26/2023 Posts: 46 Rating:
|
hello mop_s04 please see the attached picture , I've used Mod bus_Poll to find out is there any communication between camera and PC and receiving values will be possible . I can read all values at Mod bus_Poll same values in MB_client block results in a status 8383 Error reading or writing data or access outside the address area of MB_DATA_PTR. The error can occur locally as well as with the instruction "MB_SERVER. camera documentation is providing a conversion formula for ID and starting register but if i convert 1023 include attribute and instance the result will be 80141 and will result in a fault 8189 Invalid addressing of data at the MB_DATA_ADDR parameter. Regards GoAu |
Last edited by: GoAu at: 02/09/2022 22:34:08 |
|
2/17/2022 9:29 AM | |
Joined: 4/8/2021 Last visit: 4/25/2025 Posts: 640 Rating:
|
Hi GoAu, I seems that there is something wrong with DATA_PTR or DATA_ADDR parameter. I think you should check that address indicated exists on server side. https://support.industry.siemens.com/cs/ww/en/view/109755202/96379531787 The DB that store the read data should have no optimized access and also you should check that the data type of the tags inside DB and its lenght is the same as the read data. Hope it helps. Br, Cocolino |
Last edited by: Cocolino at: 02/17/2022 09:30:06Best regards, |
|
Follow us on