4/24/2023 12:59 PM | |
Joined: 9/7/2021 Last visit: 10/18/2023 Posts: 52 Rating:
|
Hello everyone. I need help from you guys. I need to solve this problem but I can't do it yet. I will briefly discuss this issue as follows. I need to control two pumps. Control principle: Running mode is alternate backup, one pump runs one backup pump with 24h rotation cycle Two modes of manual and automatic control via switch lock: - Manual mode: Use push buttons - Automatic mode: Programming on PLC Logo |
Last edited by: LuuTun at: 04/24/2023 13:01:16I can't upload the program I'm working on Last edited by: LuuTun at: 04/24/2023 13:06:16Last edited by: LuuTun at: 06/12/2023 15:53:29Last edited by: LuuTun at: 06/17/2023 23:41:26Last edited by: LuuTun at: 06/17/2023 23:44:34Last edited by: LuuTun at: 06/18/2023 00:57:52 |
|
4/24/2023 3:14 PM | |
Joined: 9/7/2021 Last visit: 10/18/2023 Posts: 52 Rating:
|
The problem is that I need to overcome the protection mode and when I load the program into the actual PLC, it doesn't work properly. |
Last edited by: LuuTun at: 04/24/2023 15:17:44 |
|
4/26/2023 3:11 PM | |
Joined: 12/24/2022 Last visit: 7/29/2024 Posts: 2 Rating:
|
Hi! try it! |
4/30/2023 3:23 AM | |
Joined: 9/7/2021 Last visit: 10/18/2023 Posts: 52 Rating:
|
Thank you. If possible, can you compress it and send it to me. |
Last edited by: LuuTun at: 04/30/2023 06:42:07 |
|
4/30/2023 3:28 AM | |
Joined: 9/7/2021 Last visit: 10/18/2023 Posts: 52 Rating:
|
Pump it fails |
Last edited by: LuuTun at: 06/18/2023 00:24:32Last edited by: LuuTun at: 06/18/2023 00:25:06 |
|
4/30/2023 9:40 AM | |
Joined: 12/18/2014 Last visit: 3/8/2025 Posts: 34839 Rating:
|
Here a possible solution from me. But you should program the buzzer function yourself, because I can't see the logic for it from your program (chaotic program structure, connecting lines criss-crossing, overlapping). I had no desire to unravel the tangle. AttachmentTwo Pumps_V2_8.3.zip (764 Downloads) |
This contribution was helpful to
2 thankful Users |
5/1/2023 10:36 AM | |
Joined: 9/7/2021 Last visit: 10/18/2023 Posts: 52 Rating:
|
IOX65. I really appreciate your enthusiastic help. |
Last edited by: LuuTun at: 06/04/2023 15:41:00Last edited by: LuuTun at: 06/17/2023 23:51:56 |
|
5/1/2023 10:51 AM | |
Joined: 12/18/2014 Last visit: 3/8/2025 Posts: 34839 Rating:
|
I knew right away that this looked familiar. Two alternate pumps with extra timerAnd what exactly is your problem now? |
Last edited by: ixo65 at: 05/01/2023 10:52:33 |
|
5/1/2023 11:34 AM | |
Joined: 9/7/2021 Last visit: 10/18/2023 Posts: 52 Rating:
|
I think not, it's actually different. |
Last edited by: LuuTun at: 06/17/2023 23:52:45 |
|
5/1/2023 11:39 AM | |
Joined: 9/7/2021 Last visit: 10/18/2023 Posts: 52 Rating:
|
This is the problem I am trying to solve.. |
Last edited by: LuuTun at: 06/17/2023 23:54:40 |
|
Follow us on