10/17/2022 11:58 AM | |
Joined: 12/22/2012 Last visit: 6/4/2024 Posts: 91 Rating: (4) |
I decided to follow sample project. Second question: If I decided to install necessary modules to side of CPU, which module is necessary for encoder input? According to their explanations, both are suitable for HSC apps. What is the difference between them? I place both to explain the situation, I will cancel the unnecessary one. These two issues really disturb me, even I experienced a lot with 1200 family. Note: the sample project is 109744840_FlyingSawBasic. I really appreciate for quick advices. . . ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/18/2022 08:08:23New subject after splitting. Division of questions into separate topics. |
|
10/18/2022 12:33 PM | |
Joined: 7/9/2015 Last visit: 5/29/2024 Posts: 3850 Rating: (564)
|
Hi, I would contact Siemens Regional Technical Consulting Partner. Contacts at SiemensRegards, Towome |
|
|
Follow us on