11/1/2010 12:52 PM | |
Joined: 1/16/2008 Last visit: 10/7/2024 Posts: 17 Rating: (0) |
For FM 350-1 Frequency Measurement & Continuous counting possible? Pl. send the sample program. |
11/2/2010 6:05 PM | |
Joined: 9/17/2008 Last visit: 8/15/2024 Posts: 49 Rating: (4) |
see attached file...it is an example of using an FM350-1 to obtain RPM. The count is also returned by the module. (FC3 and DB1) Also, there is some extra stuff in there that is irrelevant to the FM350-1. AttachmentFm350-1a.zip (1254 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on