8/9/2024 11:39 AM | |
Joined: 6/18/2012 Last visit: 8/10/2024 Posts: 35 Rating: (0) |
Hello all, I understood from the above conversation, with TIA V1x there is no separate configuration package file required. We can use the inbuilt block CNT_CTRL Block along with Data Block(CNT_CHANTYPE1). After the configuration the data not read and also i found the SF in the module. Now My question is, 1. where i can feed the encoder related parameters? 2. What is the meaning of channel address? 3. The module showing SF LED and what is the meaning? 4. I have configured in software 6ES7 350-1AH03-0AE0 but the original hardware placed in rack is 6ES7 350-1AH01-0AE0 this can be ok or not? Please find some snapshots for getting idea about the fault. ------------------------------------------------------------------------------------------ |
Last edited by: prabhakaran at: 08/09/2024 11:41:04Last edited by: prabhakaran at: 08/09/2024 12:10:48Last edited by: Moderator_Lan at: 08/09/2024 12:33:36New subject after splitting |
|
Follow us on