7/27/2019 6:07 AM | |
Posts: 6 Rating:
|
hi i have problem with my project The project was written by CFC6.2 and D7-SYS V6.2. then I install CFC V9.0 and D7-SYS V6.2. I have problem with FM458-1DP. This module does not recohnize in HW-Config. I send a Picture from HW-Config. The libraray is ok but order number of FM 458-1DP does not recognize. Can anyone help me. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/29/2019 08:14:34New subject after splitting |
|
7/30/2019 1:04 PM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating:
|
Hi, are you sure, that you try to use CFC V9.0 with D7-SYS V6.2? I am pretty sure, they are not released to be used together. |
iba AG - Data Acquisition and Analysis the way it should be |
|
Follow us on