9/8/2008 10:51 AM | |
Joined: 8/31/2005 Last visit: 7/18/2024 Posts: 2198 Rating: (328)
|
It was designed for closed loop control and aritmetics. I guess 90% of the FMs are used for drive control.
First you define a basic task time (T0) . The fastest is 100µs. Then you define 5 task times (T1 to T5). Each tasktime is a factor of 2 od T0. e.g. T0=1ms, T1= 1ms (2exp0*T0=1ms) T2=4ms (2exp2*T0=4ms, ..) You can compare it a bit with OB35 in a S7-CPU
Any standard S7-CPU Read the getting started, to get a idea who it works. |
|
|
9/8/2008 5:09 PM | |
Joined: 10/31/2005 Last visit: 8/6/2024 Posts: 366 Rating: (31) |
Thank you guys. |
9/10/2008 10:11 PM | |
Posts: 75 Rating: (13) |
You are running 2 FM458 redundant, or do you want to do this? Never heard about this. |
Follow us on