9/18/2012 4:10 PM | |
Joined: 3/16/2009 Last visit: 11/15/2024 Posts: 10 Rating:
|
Hello, Is there a way to import new fonts into WinCC for display on HMI screens? Right now it looks like my only font choices are Tahoma and Courier New.... Thanks |
9/19/2012 5:35 PM | |
Posts: 3037 Rating:
|
Hello pctguy, You can do this under the point "Runtime settings --> Language & font". Which panel do you use? Tweety |
This contribution was helpful to
2 thankful Users |
9/19/2012 5:48 PM | |
Joined: 3/16/2009 Last visit: 11/15/2024 Posts: 10 Rating:
|
Thankyou, Tweety, I found it. It looks like I can only configure two additional fonts beyond Tahoma and Courier New. Does that sound right? Is there a way to import a specific font?
I am currently using a TP900 Comfort panel. |
Last edited by: pctguy at: 9/19/2012 6:58 PM |
|
This contribution was helpful to
1 thankful Users |
9/20/2012 11:45 AM | |
Posts: 3037 Rating:
|
Hello pctguy, Yes you can configure two additional fonts beyond Tahoma and Courier New. You can choose an additional font in the list. See the screenshot. You find in this list the fonts from your operatingsystem. You need another font, you install this font under your operating system. Tweety |
This contribution was helpful to
1 thankful Users |
4/16/2014 3:38 PM | |
Joined: 12/2/2013 Last visit: 1/3/2021 Posts: 10 Rating:
|
I found that it isn't enough to select new fonts under "Runtime settings"--"Language & fonts" in the TIA portal (I use V12), you must also make sure that the very same fonts are available on the target HMI. In my case I use a TP700 Comfort Panel, which runs on Windows CE. So the trick is to also get the proper fonts installed in Windows CE. You can do this by placing a font file on a USB stick, plugging it into your Comfort panel, and then copying them into the \Windows\Fonts directory. Tap on the "My computer" icon to see and copy/paste files and folders. If you need more instructions, you can search the web for "Windows CE font install". |
This contribution was helpful to
2 thankful Users |
5/9/2014 11:16 AM | |
Joined: 12/2/2013 Last visit: 1/3/2021 Posts: 10 Rating:
|
One more thing: Files placed on the Comfort Panel don't "stick". They will be forgotten after a hard reset. Go to Control Panel - OP - Save Files to make the font files permanent. |
This contribution was helpful to
3 thankful Users |
We are working on a new user interface with better overview and more relevance.
Follow us on