Industry Online Support
Technical Forum
10/28/2014 4:32 PM | |
Posts: 767 Rating:
|
Hello pattanaik, Rating for a servo drive is output voltage and output amps. Nominally you could approximate this to rated power for a three phase output to be: AC three phase amps to kilowatts calculationCalculation with line to line voltageThe power P in kilowatts (kW) is equal to square root of 3 times the power factor PF times the phase current I in amps (A), times the line to line RMS voltage VL-L in volts (V) divided by 1000: P(kW) = √3 × PF × I(A) × VL-L (V) / 1000 Deputy |
Follow us on