Industry Online Support
Technical Forum
4/23/2010 4:15 PM | |
Posts: 1 Rating:
|
I would like to know if I can found a product to install directly on S7-400 Chasis to connect a foundation fieldbus network? Thanks in advance, |
4/23/2010 7:33 PM | |
Joined: 9/27/2006 Last visit: 8/5/2024 Posts: 12273 Rating:
|
Hello nanuss; Up to now, there is no such rack-mounted module for the S7 family (rumors are being spread about something for H1 coming this summer, but no confirmation yet!). However, there is a DP/FF link that you could look at: From the manual “DP/FF Link” found on the following link: http://support.automation.siemens.com/WW/view/en/24239833 The DP/FF Link consists of the following components: ● Anybus DP Link (pre-configured; the configuration for PROFIBUS DP cannot be changed) ● Fieldbus Interface Module (FIM3420) (configurable to suit corresponding applications) Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/23/2010 9:30 PM |
|
Follow us on