Industry Online Support
Technical Forum
4/26/2007 6:34 PM | |
Posts: 297 Rating: (41) |
Yes, it is possible to access a flash drive attached to the USB port, if the PCU 50 is running Windows XP. One method that allows both floppy and USB access is to purchase the DNC Machine option. Even if you don't use a network, you can define a soft key for the drive G:. The other method changes the function of the Disk/Card soft key from floppy to USB drive. This requires a re-boot, and this does not allow access to both sources. Refer to the article found at http://support.automation.siemens.com/WW/view/en/19074127for details. You may have to change the name of the section from [Services] to [Dienste] for this to work. HTH, SteveA |
4/27/2007 12:01 PM | |
Joined: 4/26/2007 Last visit: 8/15/2024 Posts: 120 Rating: (8) |
Hi, I dont need floppy, but it is present on maschine. So it must running. Can You look at attachment? Attachmentdrive connection via MD.pdf (1152 Downloads) |
Follow us on