2/22/2018 4:15 PM | |
Joined: 8/3/2009 Last visit: 8/1/2024 Posts: 13425 Rating: (1702)
|
Hello unfortunatelly there is no automatic FTP Client functinoality implemented in the Simatic Panels. Also not in current Comfort Panels. Here is the way to use manually a FTP function (FAQ is old but also today the only way with FTP) https://support.industry.siemens.com/cs/ww/en/view/15250466 The most Usecases like yours are solved with this way of integrating the Panel: https://support.industry.siemens.com/cs/ww/en/view/92346478 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on