6/28/2014 2:03 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello shaun Please check the Local bits may be being assigned as a byte / word / double word. e.g. look for statements like L xxx T LB 68 or LW 68 etc Many times Controlbits / Status bits are stored as bytes / words and used as individual bits after transferring them to a byte / word in the local area. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
6/28/2014 4:33 PM | |
Joined: 12/22/2005 Last visit: 10/29/2022 Posts: 18 Rating: (0) |
Hi William B, Attached please find a .pdf of the FB. I can also supply zipped FB if it will make more sense. Thanks in advance.
AttachmentFB721.pdf (245 Downloads) |
Follow us on