1/22/2014 8:00 PM | |
Posts: 510 Rating: (117) |
Here are two options: http://support.automation.siemens.com/WW/view/en/56749384 http://support.automation.siemens.com/WW/view/en/66839614 Good Luck billwest |
1/22/2014 8:12 PM | |
Posts: 5 Rating: (0) |
thanks Bill the one you show me is for 1200, any difference if i am going to use S7-300 or PCS7? |
1/22/2014 8:19 PM | |
Posts: 510 Rating: (117) |
Ok How about this one http://support.automation.siemens.com/WW/view/en/63042779 billwest |
1/22/2014 8:32 PM | |
Posts: 5 Rating: (0) |
Hi Bill do you have the face plate for TIA V11? thanks |
1/22/2014 8:50 PM | |
Posts: 5 Rating: (0) |
Bill when I open the one you gave to me in TIA V11, there are no "stop","Auto", and "remote" buttons on the face plate. why? thanks |
Follow us on