Industry Online Support
Technical Forum
10/4/2012 7:33 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi well for your first question , See there are two parts for the memory of S7400 controller system. One it has intergrated memory and another expandable memeory. Normally the intergrated memeory shall be few Mb and user has to expand the memory size using RAM or Eprom's. Normally your program gets stored in the Feprom or RAM as the present size is not sufficent for the program is conserned. For the Second Question. Minmum requirement is 1 MB of RAM or Eprom shall be sufficent for small application. For further questions, Refer S7400 document. Have fun... |
Jazz |
|
Follow us on