11/13/2013 8:50 PM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating: (9) |
And CU's of FW2.x are they compatible with motormodules of FW4.x? |
11/14/2013 4:33 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
Hello, yes CU FW V2.x can Handle the new motormodules, i remeber since Version V2.5. Regards Christoph |
11/6/2015 12:07 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
Hi, yes this is no problem.
Christoph |
11/6/2015 12:13 PM | |
Joined: 8/6/2013 Last visit: 1/11/2024 Posts: 3 Rating: (0) |
Wow! Thanks a lot for the swift reply^^ Regards Marius |
Follow us on