9/14/2015 11:51 AM | |
Posts: 3 Rating: (0) |
Hi all. In my project i have:
I can show in HMI the speed setpoint and the actual speed, using Motion Control blocks (MOVEJOG, p.e). And i want to show in HMI the actual values of:
My question is: How can I "receive" those parameters in PLC to show them in HMI? See my attachments. Regards. AttachmentG120 CU240.zip (399 Downloads) |
9/14/2015 12:21 PM | |
Joined: 11/29/2011 Last visit: 8/19/2024 Posts: 1359 Rating: (232) |
Hi, There is an easy way to display VFD data on HMI. See this: SINAMICS G/S: HMI direct access I hope I could help! |
- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to1 thankful Users |
9/4/2020 8:44 PM | |
Posts: 10 Rating: (0) |
Do you have an example of the move, cause I got lost in the explanation Thanks |
Follow us on