8/26/2022 3:44 AM | |
Joined: 5/5/2020 Last visit: 8/26/2022 Posts: 18 Rating:
|
hello I am using the sinamics g120 frequency inverter with mobdus communication How can I do speed control with an encoder and a plc s7 1200 What parameters would I have to configure in the drive? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/26/2022 10:22:41Text formatting optimized. Last edited by: Jen_Moderator at: 08/26/2022 10:24:53New subject after splitting. |
|
8/27/2022 3:37 AM | |
Joined: 4/23/2010 Last visit: 1/29/2023 Posts: 7962 Rating:
|
Please refer below application examples. SINAMICS: Speed control of a SINAMICS with a SIMATIC S7 via MODBUS SINAMICS G120 converter with Control Units CU230P-2; CU240B-2; CU240E-2 |
Follow us on