7/19/2019 3:25 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665) |
Hello Sanket; The CPU 315-2PN/DP can act as an IO Controller over Profinet, so it can read and write to any Profinet IO Device, such as a G120. There are many Application Examples on the forum showing how this can be done (depending on the thé specific controller, the programming environment and the requirements for ProfiSafe exchanges, if needed. Here is a basic one, designed for Step 7 v5.5: SINAMICS G: Speed control of a G120 using S7-300/400 (STEP 7 V5) with PROFINET (FW3.2) https://support.industry.siemens.com/cs/ww/en/view/45287261 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 07/20/2019 11:53:10 |
|
This contribution was helpful to1 thankful Users |
Follow us on