Industry Online Support
Technical Forum
10/1/2014 4:51 PM | |
Joined: 9/12/2014 Last visit: 9/18/2024 Posts: 4 Rating: (0) |
How can I communicate esa vt525w vith siemens g120 driver |
10/6/2014 12:33 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello rodyan2@gmailcom, these HMIs are in PROFIBUS versions available so by choosing a G120 e.g. with a CU250S-2 DP a communication via a S7 controller is possible. Examples with a SIMATIC HMI: http://support.automation.siemens.com/WW/view/en/34677186/136000&cspltfrm=30&cssw=0&csbinh=8 If the HMI is a DP Class2 Master, a direct DP communicationwith an actual drive (firmware 4.7) is possible. For details please contact your local Siemens representative and the manufacturer of the HMI of course. |
With best regards, |
|
Follow us on