12/5/2022 1:05 PM | |
Joined: 3/27/2008 Last visit: 3/18/2025 Posts: 1180 Rating:
|
Hi try this For fixed setpoint: P1020 = 722:0, (fixed setting); P1001 = 1179rpm? ( check this); P1025 = 840:0, ( on/off command, DIN 0, terminal 5 High); P1070 = r1024. P1113:0 = 0, (remove setpoint inversion); PI Technology controller: P2200 = 722:1, (enable PI controller); P2253 = 2201, (fixed value 10% default); P2201 = fixed value for Pi setpoint); P2264 = 755:0, (analogue input, terminals 3/4, process variable); See, attached for a view of the PI controller. AttachmentG120C PID control.pptx (513 Downloads) |
Last edited by: Tractor at: 12/05/2022 13:06:43Last edited by: Tractor at: 12/05/2022 14:25:08Tractor |
|
This contribution was helpful to
1 thankful Users |
12/5/2022 3:03 PM | |
Joined: 4/21/2016 Last visit: 2/10/2025 Posts: 12 Rating:
|
Thankyou, it works! |
This contribution was helpful to
1 thankful Users |
12/5/2022 4:58 PM | |
Joined: 3/27/2008 Last visit: 3/18/2025 Posts: 1180 Rating:
|
'Cool', thanks for the feedback. Tractor |
Tractor |
|
Follow us on