4/27/2016 9:27 PM | |
Posts: 15 Rating: (0) |
Is there any other value that is not writable in logo8? |
4/28/2016 6:07 AM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33757 Rating: (4191) |
In attachment there are the parameters. AttachmentLOGO! 8 Soft Comfort Online-help sides 109-119.pdf (248 Downloads) |
This contribution was helpful to1 thankful Users |
4/28/2016 11:58 AM | |
Joined: 10/10/2010 Last visit: 4/28/2024 Posts: 307 Rating: (15) |
so if i need to change the speed of a motor by HMI directly from logo to variable speed drive ? what should i do? |
4/28/2016 12:16 PM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33757 Rating: (4191) |
In attachment a little screenvideo. Every parameter of an block ist writable, when it shows an icon with sheet and pencil. AttachmentVM.wmv (290 Downloads) |
4/28/2016 2:53 PM | |
Posts: 15 Rating: (0) |
fantastic explanation. |
Follow us on