6/24/2016 10:01 AM | |
Posts: 2 Rating:
|
Thanks, I had the same idea, that I could export DB's as source files, tamper the files and load back to the program. But the problem is that the data is not included in the AWL files, so where can I manipulate the data? I have attached an instance DB source file which was generated after changing message text in the instance DB. The message text is not included. Attachmentmotor_iDB_600.txt (64 Downloads) |
Follow us on