12/7/2018 4:03 PM | |
Posts: 1 Rating: (0) |
Hello, For the first time I am working with the Iot 2040 and azure. I followed the tutorial and the OPC UA part works. I can also run the createdeviceidentity.js and then I get the device ID and Device Key as it should be. I have entered it all in the application_example.js, but if I excecute this I get an error message when it tries to connect to the Azure IOT hub. As shown in the image Is there anyone who can help me with this? With kind regards Bas ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/10/2018 8:11:31 AMNew subject after splitting |
|
12/10/2018 1:02 PM | |
Joined: 4/28/2015 Last visit: 5/15/2024 Posts: 3345 Rating: (377)
|
Hi, have you checked your IOT2000`s system time? There was also a problemr with Azure IoT Hub node-red nodes and the guy had the same error using amqp. Setting the right time on the IOT solved this problem. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
1/2/2019 1:34 PM | |
Posts: 4 Rating: (0) |
You should go through the Internet of things application which is specially used to send the wireless temperature sensor data to azure IoT hub - https://ncd.io/getting-started-with-microsoft-azure-and-wireless-temperature-humidity-sensor/ I hope this will surely help you out. |
This contribution was helpful to1 thankful Users |
Follow us on