6/9/2014 11:49 AM | |
Joined: 6/3/2013 Last visit: 6/10/2024 Posts: 7 Rating:
|
Hi there, I'm facing similar problem here. I've no problem using the Get if both PLC is under the same project file with my own programming. But if I wish to access client's PLC whereby client only provide me the PLC IP address and DB number of their PLC, can I use the same way to get the data exchange between the PLCs? I wrote 2 simple program in different project to test, then I use either of it to put the Get instruction and trying to pull the data of the other PLC. It doens't work. Both DB on both PLC are identical, "standard DB". Screenshot of my configuration attached. Anyone can advice?
Attachmentscreenshot.zip (334 Downloads) |
Last edited by: Narrator1 at: 6/11/2014 1:51 PMTopic split from /tf/WW/en/Posts/74028 |
|
6/10/2014 2:22 PM | |
Joined: 7/7/2010 Last visit: 7/24/2024 Posts: 14996 Rating:
|
See attached. This is where the s7 subnet ID is configured. Please post your results. |
science guy |
|
6/12/2014 8:56 AM | |
Joined: 6/3/2013 Last visit: 6/10/2024 Posts: 7 Rating:
|
It still doesn't work after I set the profinet name same as the client PLC. Previously I've done other program using this GET instruction as well, but in that program both PLC were under my control in the same project. I check the profinet address properties, I found that in that previous project when I link up both PLC there is more details on the properties, it has those info like rack and slot number. But for this, it doesn't. Those rack, slot and others info are blank. Any things else need to set? Perhaps you I attach the program if it's still unsolve and you have a look? TQ very much.
AttachmentAddress Details.zip (194 Downloads) |
Follow us on