6/28/2019 9:48 AM | |
Posts: 5 Rating:
|
Hello, members of this tread We have basically the similar problem mentioned above.
When we try to change the SW logic for controling the drive (just for testing purpose), means first we set the signal for traversing and than set the enable bit, it works well and no alarm appear. But this is not solution for me (cannot change the customer standard blocks). These things drive me crazy, any idea what to do or check next?
------------------------------------------------------------------------------------------ Attachmentdoc1.pdf (312 Downloads) |
Last edited by: The Helping Hand at: 06/28/2019 11:40:53New subject after splitting |
|
6/28/2019 10:33 AM | |
Joined: 10/11/2006 Last visit: 3/19/2025 Posts: 5999 Rating:
|
Hello, < Firmware Version 4.7 HF11 no alarm 7496 occurs. With Firmware Version 4.7 HF11 this is fixed, and if position controller is not enabled 7496 occurs. In general: It is helpful to use SinaPos for controlling Basic Positioner. https://support.industry.siemens.com/cs/ww/en/view/109736845 |
With best regards, |
|
7/1/2019 9:52 AM | |
Posts: 5 Rating:
|
Hello Technology team, thanks for your answer. I had tested firmware version 4.7 HF11 (Internal version ID V04.70.35.24), and also had tested firmware version 4.7 SP6 HF5 (Internal version ID V04.70.83.19) neither one works well. I´m still getting Alarm 7496 EPOS: Enable not possible. Now we are adding two new one G120 CU250D (ordered and bought in 2019) and getting this alarm!!! For our purpose it is still not working. |
9/8/2021 12:25 AM | |
Joined: 11/17/2013 Last visit: 10/8/2024 Posts: 11 Rating:
|
Hello all, it is 2021, Tia v16 and I am facing exactly the same problem. Anyone found a solution to suppress this message? |
Last edited by: ser85 at: 09/08/2021 00:27:07 |
|
We are working on a new user interface with better overview and more relevance.
Follow us on