2/19/2025 8:18 AM | |
Joined: 2/4/2020 Last visit: 3/6/2025 Posts: 44 Rating:
|
So let's say I have to use a scriptblock for some function. if i write that command inside the query function, it will load that object again and again for all the rows, is there a way to define this object(scriptblock/bas object) in such a way that it is executed only once ? |
2/19/2025 1:20 PM | |
Joined: 10/23/2023 Last visit: 3/18/2025 Posts: 9 Rating:
|
Hi do you know the script functions in the options tab? Maybe you can execute a script there once.. BR |
2/20/2025 6:22 AM | |
Joined: 2/4/2020 Last visit: 3/6/2025 Posts: 44 Rating:
|
Yes, but the variables declared there are not accessible in query column scripts (unless I use workset.globals which I want to avoid) |
2/24/2025 4:44 PM | |
Joined: 6/3/2022 Last visit: 2/24/2025 Posts: 12 Rating:
|
I can think of three options, no of which are perfect:
|
We are working on a new user interface with better overview and more relevance.
Follow us on